Hello,
According to the spec sheet the current limit on the TPS2121 varies +/- 0.5 A. There is an equation used to calculate the current limit based on the current limiting resistor used [ I = 65.2 / (R^0.861) ]. I have used various resistors including those greater than 100 K to get current limits below 1 A and the measured current limit is very close to the calculated value (within 100 mA). The current limit also does not vary much with temperature (-40 to +85 C) and between the 2 chips I tested.
So my question is, why does the spec'ed current limit vary +/- 0.5 A? Is it mainly due to chip to chip variation, variation due to temperature, or something else? I ask because I am looking to lower the current limit below the 1 A spec., to 0.8 A or lower, and so far have not encountered any issues by simply increasing the resistor value.
Thanks.