Other Parts Discussed in Thread: LM25145
Hi Team,
Just want to check the eff on 19Vin to 12Vout, 150W. Thanks.
BRs
Given
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ding,
Thanks for the question. You can use the LM5145 quickstart calculator file to check efficiency and power losses. With 30V or 40V NexFETs, > 95% should be achievable.
Note that if Vin-max < 42V, you can use the LM25145.
Regards,
Tim