Part Number: ISO5452
Dear team,
See from datasheet of ISO5452, RDY could self-recovery, but FLT only recovery by reset RST. In customer's application, FLT usually means serious fault, they will not want to reset DESAT, they will cut off the end equipment and then power up the machine. Please help confirm:
1. Is the way customer deal with FLT fault if right or wrong?
2.Did the FLT fault disappear when power on again? Could customer connect RST directly to 5V?
3. Any other way recommend to deal with the fault?
Thanks.
Best regards,
Sammi