Dear expert,
Can BQ76940 support balancing with transistor instead of FET? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear expert,
Can BQ76940 support balancing with transistor instead of FET? Thanks.
Hi Minqi,
Yes, the BQ76940 could support BJT transistors for balancing instead of FETs, but balance current will typically be lower than with a FET. Due to the architecture of the BQ76940 the input resistance must be large to keep the part powered during short circuit events as described in https://www.ti.com/lit/pdf/slua749 , so the base current will be low and even with high gain transistors the balance current may not match what is available from a FET using a single transistor. You could use the BJT to control the base of a second BJT for higher gain, or a MOSFET to get the full cell voltage for Vgs and thus lower RDSON and higher balance current. This is more components, I don't know of an available example.