Hello, is the output pin state defined for VCC below min operating 4.5V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Francisco,
The UCC27322-EP is defined for 4.5V < VCC < 15V rail-to-rail operation.
Using the driver IC outside of the recommended operating conditions might impact the driver's switching behavior and/or performance.
Regards,
-Mamadou
Understood. My question is whether the output is floating or in what state during power up or power down when Vcc is less than 4.5? Wish it had an undervoltage lockout feature but it does not appear to be the case.
Yes, I checked the datasheet, and it doesn't have an UVLO protection block.
However, Figure 23- Figure 26 from the datasheet will give you a lot clue on what happened during VDD power up and power down.
Best regards,
Wei