This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63070EVM-693: it does not work if Vin less than 3V

Part Number: TPS63070EVM-693
Other Parts Discussed in Thread: TPS63070, TPS63802


I am testing the ev board in the following conditions:
Vin = 2.5V
Vout desire= 3.3V
Rload= 15 ohm

JP1 Enable: HI
JP2 Vsel: LO (3.3V)
JP3 PS/Sync: HI

The problem is that Vout is 2.4V (139mA) instead 3V3 (220mA).

I try also JP3 PS/Sync: LO but i have the same results 2.4V (139mA).

If i try Vin = 3V, Vout is, correctly, 3V3 (220mA).

I need to have 3.3V if I put about 2.3 / 2.5 V in input.

What is the problem? Does the board have a problem or is the datasheet wrong?
How can I make the system work? Can you advise me to change some component to make the system work in my condition?

best regards.