This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25892: Is this charger PD compatible?

Part Number: BQ25892


Hi team,

Is this PD compatible if I were to use a front end PD chip?

  • Hi Lauren,

    This charger can only communicate with USB BC1.2 adapters and other select HVDCP adapters up to 14V and 3.2A.  If host software can limit the USB type C PD output below 14V, then yes this charger is compatible.  It has its own input current limit with max setting of 3.2A. 

    Regards,

    Jeff