Other Parts Discussed in Thread: USB2ANY, TPS55288, , TPS55288-EVM-GUI
I have a new TPS55288 EVM board, and a new USB2ANY. I have the program up to work with the TPS55288, and the GUI Composer has been loaded. However the program (which appeasr to be called simply "TPS55288") always says "Hardware not Connected" when I try to connect. The green LED on the USB2ANY is on.
Questions:
1) Do I have to have the USB2ANY plugged into the EVM board for the connection to be made?
2) If yes, does the EVM board need to have power applied at the input?
3) Should I be able to see the USB2ANY in the Device Manger on a PC (running up to date Windows 10) ?
4) What are the next steps I need to take to resolve this problem ?