Can the LM5069 be used upstream of the plugged-in board? All the examples I see use it at the immediate entry of the PCBA plugged into a live backplane. Can the LM5069 be used on the backplane, to allow hot swapping of downstream connections?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can the LM5069 be used upstream of the plugged-in board? All the examples I see use it at the immediate entry of the PCBA plugged into a live backplane. Can the LM5069 be used on the backplane, to allow hot swapping of downstream connections?
Hi,
What is your downstream circuit consists of - is it a DC-DC converter ? How much is the input capacitance of your downstream circuit ?
LM5069 can be used on the backplane as well. However, hot-plugging a downstream with a large capacitance could cause circuit-breaker event due to capacitor inrush currents and restarting the LM5069 output.
Best Regards, Rakesh
Thanks for the quick response. I'm designing a power distribution box for many of these downstream loads. I'm not completely sure what each downstream circuit is, as they are off the shelf systems consisting of a motor and resistive load. Probably a reasonable assumption that there is some bulk input capacitance. In addition, it is connected via ~2+ meter cables which will add cable capacitance.
I think you're right that the potential CB event might be too difficult to manage.