Hello,
The datasheet of UCC28180 says that Max Vcc Turn ON threshold is 12.1V. I was wondering if it would be okay to use a 12V supply with output tolerance +/- 100mV for it (Using a 12V fixed output LDO).
The recommended VCC input voltage from a low-impedance source is recommended as VccOFF+1V leading to worst case scenario need of 11.3V which is not in sync with the above statement. Would you recommended going for a 12V supply with the above given specs for an automotive product?