This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R2: QMAX update is not working with OCVFR bit set

Part Number: BQ40Z50-R2


Hello everyone,
I am using the bq40z50-R2 for a 3S1P battery. Afterwards I performed a successful learning cycle I reduced the charge voltage in the golden image to 4.1V per cell because this is given by the application. Now the QMAX update does not work anymore and the OCVFR bit remains set if the battery is fully charged.
Is it possible that I am still in the flat region with a charge voltage of 4.1V per cell? I use the Chem ID 0x2481. Is there a workaround if the flat region is really that big?

best regards
David