Hi,
Is there a battery discharge protection function on BQ24172?
If not, which protection IC is recommended in this case?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Is there a battery discharge protection function on BQ24172?
If not, which protection IC is recommended in this case?
Thank you.
Dear Cindy,
The Q2 FET will prevent input discharge protection from the battery. Separate protection is required from battery discharge to the load. Are you using a pack with a protector or bare cells? If you are using bare cells, I would recommend searching through the TI battery protector site below.
http://www.ti.com/power-management/battery-management/protectors/overview.html
Thanks,
Mike Emanuel
Please click "This resolved my issue" button if this post answers your question.