When I executed global command 30h+AAh+temp address writing to two tps23861 chips with daisy chain configuration, only one chip is written into temp address successfully while another failed. Here are some questions :
1: If it is due to an improper up-pull resistor (1k ohm) for SCL and SDAO that caused failure of writing to two chips simultaneously.
2: If the global command 30h is influenced by A3 and AIN?