Other Parts Discussed in Thread: LMR14030, LM5088, TPS2546
Hello Community,
Hope the lockdown's going good for all!
I was designing a USB charge control IC based on the TPS2549 IC.
The datasheet's application note mentions a design procedure for CS pin feature available with the LMR14030 Buck IC.
However in my application I am using the LM5088 Buck IC.
I have problem in computing the exact values for R-FA & R-FB for which the V-CS > 2..5V condition can be met appropriately.
The O/P voltage for LM5088 can be set via the following equation:
RFB2/RFB1 = (VOUT / 1,205) -1
The V-REF is 1.2V
The VOUT is 5.7V, RFB2 = 6.49K & RFB1 = 1.74K. Now RFB1 = RG = 1.74K for TPS2549 calculations. RFB2 = R-FA + R-FB
The calculations are below assuming Wire resistance = contact resistance = 0R.
Calculation for TPS2549
|
The criteria for V-CS is > 2.5V which is needed for this calculations.
I tried using some combinations of equations to get RG, RFA & RFB values in some range and try out but I am getting negative values for RFB.
Has anyone tried using the LM5088 with the TPS2549? Any suggestions on what can be done here to get deliverable results?