This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53319: About EN pin

Part Number: TPS53319


Hi,

Customer is trying to control sequence by controlling EN with CPLD

Customers connect the EN pins of multiple devices to one signal source.
In the background, customers are looking into pull-up resistor constraints.

1.Does TPS53319 have a Zener diode and pull-down resistor inside the EN pin?
  Could you tell me the Zener voltage and pull-down resistor value?

2.When dividing the control voltage of the EN pin externally,
  Is there a restriction on the voltage dividing resistor value?
  Customer is using a pull-up voltage of 12V. This voltage is divided to 3V.

3.Please advise on the precautions when sharing EN signals with multiple devices.

Regards,
Yusuke