Other Parts Discussed in Thread: BQSTUDIO
Hi,
Does the following parameters have to be scaled according to the current scaling?
- Res Current;
- Dsg Current Threshold;
- Chg Current Threshold;
- Quit Current.
For example I have current scale of 4, a 4A current is calibrated to be seen as 1A by the gauge. Shall I divide the standard values of above parameters by 4 also?
Bonus question: My expected End of Charge current is 168mA, which leads to a taper current of 42 with the aforementioned scaling. FC set is -1 to use the full charge detection algorithm depicted in paragraph 7.3.11 1) of the datasheet. Is a Chg Current Threshold set to 40 is low enough to ensure the gauge will have sufficient time to set FC?
Best regards,
Jérémie