Hi,
I have a WIFI module on-board a processor baseboard. This module is the only 3.3V device on the board and I didnt want to use a dedicated buck circutiry for it since that will increase expenses.
The average current draw is around 200mA and its not a battery operated deviice (meaning that effciecny is not a concern) and the system is well ventilated . Is there any other reason why I should consider using a buck converter for RF WIFI modules with integrated PA?
Regards,
Tony