Part Number: BQ40Z50-R3-DEVICE-FW
Tool/software: Code Composer Studio
Hi, BQ40Z50-R3 I found was a firmware only type, and its specification manual says that it is able to flash into any exsiting BQ40Z50 hardwares (like BQ40Z50-R2, BQ40Z50-R1 or BQ40Z50); How should I do to burn BQ40Z50-R3 into BQ40Z50-R1?
PS: I downloaded and installed bq40z50R3FirmwareBundle-3.09-windows-installer.exe already.
When I connected to BQ40Z50-R1 via EV2400, it was identified as R1.
If I manually chose BQ40Z50-R3 in advance, the R3 interface would appear, but there was a warning of no respond of the device and then it would change to R1 automatically.
Is there any detailed instruction for flashing R3?