Hi,
I am using ISO5852 device for 1700V SiC (C2M0045170P_CREE). and topology is full-bridge converter.
VCC and VEE are + 15V / -5V, and the Miller clamp pin is not used.
When the input voltage of converter increased, a cross talk issue occurred in which the gate voltage of the upper switch increased when the lower switch turned on.
When I connect the Miller clamp pin to the output of IC, it seems that the crosstalk issue disappears.