Other Parts Discussed in Thread: TPS54302
Hello guys,
One of my customers is considering using TPS54202H for their next products.
They found the following description on page 11 in the device datasheet (SLVSDG7).
"7.3.11 Bootstrap Voltage (BOOT)
The TPS54202H has an integrated boot regulator and requires a 0.1-μF ceramic capacitor between the BOOT
and SW pins to provide the gate drive voltage for the high-side MOSFET. A ceramic capacitor with an X7R or
X5R grade dielectric is recommended because of the stable characteristics over temperature and voltage. To
improve drop out, the TPS54202H is designed to operate at 100% duty cycle as long as the BOOT to SW pin
voltage is greater than 2.1 V typically."
They want to know how to achive 100% ON duty.
Could you please tell me the way or any reference schematic for 100% duty?
Also could you please give me your reply for the following question?
What is the maximum ON duty or the minimum OFF duty (or time) in normal operation of TPS54202H?
Because the customer want to know what input voltage is needed to output 15V.
Your reply would be much appreciated.
Best regards,
Kazuya.