Other Parts Discussed in Thread: CC1101, MSP430FR5994
I want to monitor the current consumption of a smart meter with IOT communication. It should work with a small 3,6V Li-SOCL2 battery for many years.
When all the communication is off, the resulting current is smaller than 10uA. When the IOT wakes up, we could have very short pulses up to 800mA for several mS each (an additional capacitor protects the battery from the pulses). The problem is that we don't know when they occurs. The integration of the sleep current and the IOT current gives us an average current of nearly 50uA.
Now we search a device to predict the state of the battery (coulomb counter). If I read the datasheets, it seems to me that all the coulomb counter needs a current of approximately 100uA, when they are on. Is that right? Because in that case, the coulomb counter will need two third of the battery capacity.
Without CC: 2600mAH at 50uA average => 6 years for one Battery
With CC: 2600mAH at 150uA average => 2 years for one Battery
Please could you help me to better understand the work of a coulomb counter with an IOT device, where we don't know, when the pulses occurs. Witch one could you advise us to use for this application?