Hi team.
My customer is currently working with BQ25892 wanted to know some clarification.
1. If the VBUS input is zero or not connected, and the battery is already full, does the battery back power the IC?
2. Can it detect a reverse battery polarity? How?
3. There is a pin, /CE or Charge Enable pin. If I toggle this pin to LOW, it charges the battery. If I toggle this pin to high, does it disengage the BAT and SYS pin and put these pins to high impedance?
4. In the specs, on page 6, it shows this, regarding the /CE pin, "Battery charging is enabled when CHG_CONFIG = 1 and CE pin = Low." What happens if I put the CHG_CONFIG = 0 and CE pin = Low? Does it have the same effect as CHG_CONFIG = 1 and CE pin = HIGH?
Thanks in advance.
Renan