This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55340: TPS55340

Part Number: TPS55340
Other Parts Discussed in Thread: LM5122,

I use TI-PMLK Boost Kit

Have no problem with LM5122, but when i start Lab-3 test-1 with TPS55340: no switching, no regulation Vin=Vout on any Vin and Load 

  • Hi Ilia,

    Thank you for using the boost kit.  It sounds like the board connections are not set up correctly. Please double check the connections. If the connections are correct but you still do not see it work, then the circuit is somehow damaged.  ESD can be a common reason to kill an IC.  Note that this kit has been released for several years and this is first time we heard about such issue. 

    You may also contact Dr Femia.

    Best Regards,

    Youhao Xi, Applications Engineering.