This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61040 - Efficiency??

Other Parts Discussed in Thread: TPS61040

I am using TPS61040 for Driving small OLED Display - 96 X 128 Pixel.

Parameters are as foloows:

Input Voltage: 3V

Output Voltage:  12V

Load Current: 2mA@12V

Input capacitor - 4.7uF

Output Capacitor - 1uF

FB Capacitor - 22pF

Inductor          - 10uH

R1 - 2.2M

R2 - 270K

Output voltage generated is close to 12V, 200mV ripple.

Problem: Earlier I was using LT3464. This circuit use to draw very close to 10mA current from 3V supply.

With TPS61040, current is 13mA without any load and 90mA!!

Awaiting suggestions

Vimal Amin