Hi team,
My customer is evaluating TPS259827L with our EVM (TPS259827LEVM). They configured the EVM for 15A current limitation and apply a 24V input power supply. The problem is the system cannot start up if they connect a 2.4 ohm load resistor on output (the output is 0V). While it can start up correctly if removed the load resistor. What is wrong? how should they configure the EVM to make the efuse start up with 10A load?
Here is customer's EVM configuration:
J4: OPEN
J9: 5-6
J10: 7-8
J6: 1-2
J11: OPEN
J8: SHORT
J7:2-3
Thank you!
John