This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS548D22: Frequency curve

Part Number: TPS548D22

Hi TI,

please help to provide frequency curve of TPS548D22.

1. frequency vs output current

2. frequency vs output voltage

Thanks,

BR

  • Hi ,

    Data I found for this are in the images below.

  • One more set of data I just found to help show the fsw vs Vout is below. Operating near the minimum on-time causes the fsw to start to decrease with the 0.6V output with 12-V input so data at 6-V input is also given.

      Vin = 12 V, Vout = 0.6V, Iout = 5A Vin = 6 V, Vout = 0.6V, Iout = 5A Vin = 12 V, Vout = 1.0V, Iout = 5A Vin = 12V, Vout = 5.5V, Iout = 8A
    Set Fsw (kHz) Fsw (kHz) Fsw (kHz) Fsw (kHz) Fsw (kHz)
    315 317.7 301.8 314.0 290.4
    425 428.8 405.0 428.3 387.8
    550 519.1 509.9 545.1 486.9
    650 581.7 613.4 658.6 582.6
    825 649.9 767.6 806.2 725.4
    875     883.8 828.7
    1050     977.6 975.6
    1125       1166.2