Hi,
I am looking to build a programmable single laser drive. I need a variable output current between 50mA and 400mA to change the laser output power intensity programmatically. I would prefer Analog dimming over PWM dimming because the laser output is used for imaging a surface with a 100fps camera. (I would think PWM dimming would work at high frequecy(100kHz+) for the use case though with a MOSFET drive, But suggestions are welcome). Laser forward voltage will be around 2V. Input can give 5V, 2A. Its a price sensitive part so ideally would like to optimise for price as well.
Is there a single TI part I can look into for this specific application?
Thanking you in advance.