Other Parts Discussed in Thread: TPS61194
Hi Team,
My customer now use the TPS61194 to boost 12V to 24V and output current is 4*90mA.
They found that inductance of TPS61194 is howling when PWM frequency is 1kHz/10kHz.
If the PWM duty cycle is 100%, the inductance is not howling.
Customer also change the inductance to the following value, but still howliong.
600KHZ 22uH /2.6A
300KHZ 47uH/2A
1300KHZ 10uH/2.6A
The SCH is as following:
The LCD: