This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: The real capacity is greater than the max design capacity in bqstudio

Part Number: BQ40Z50-R1
Other Parts Discussed in Thread: BQSTUDIO, BQ40Z80

Hi,

 I am using the bq40z50-r1 with the 4S17P battery,the single cell capacity is 5000mAh,so the design capacity should set 85000mA,but the max value of the design capacity in bqstudio is  32767mAh.The real capacity is greater than the max design capacity in bqstudio.I can not write the value and do the learning cycle. 

Can I change the scale???How should I solve this problem???