Other Parts Discussed in Thread: TPS54302, TPS563201, TPS56339
Hello
I have a question concerning the technical specification of TPS54331.
I habe an circuit where the Input Voltage is: 4.5 to 9V and the output voltage is 3.5V.
Maximum current 2.2A
In the datasheet there is an example circuit:
V_in is limitted from 7-28V. Why is this the case.What happens if the input voltage goes down to 4.5? What do I have to change for Input 4.5 to 9 when output should be 3.5?
What limitates my input voltage?
Best regards