This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS659037: PWRDOWN pin delay

Expert 4455 points
Part Number: TPS659037

Hi PMIC team,

My customer is using TPS6590378, PWRDOWN is configured as active High, SWOFF_DLY is set to 0 and they want to trigger a power cycle using Sitara processor. However, they observe that pulling PWRDOWN pin high for 8ms does NOT trigger a power cycle. If they increase the high-time to 16ms, the TPS6590378 initiates a power-down sequence. Following questions arise:

   Is there some debounce filter internally for this PWRDOWN input?

   What is the minimum pulse time needed for PWRDOWN pin, in order to do a power cycle of PMIC?

   How much can this minimum pulse time vary between different devices and in worst case?

Thanks & best regards,

KF

  • KF,

    How long after you turn on the device are you trying to turn off the device? Once the device is turned on, it takes up to 15ms for OTP settings to load and power up. Then the device is available to shutdown. Can you scope how long the device is on?

    Also, how are you turning the device on? Which pin?

    PWRDOWN has a typical 2ms debounce time.

    Thanks,

    Nastasha

  • Hello.

      It does not matter the time for turning off using PWRDOWN, after turning on. It can be even minutes.

     PWRON and RPWRON methods for ON request are not used (PWRON Not Conn., RPWRON tied to 1.8V = SMPS8). For power-ON, the device is powered by 3.3V; after 3.3V stabilization the RESET_IN pin is released and device powers on.

     In our design we want to trigger PWRDOWN using RESET_OUT from Sitara, which is a 7.6ms pulse. Applying this at PWRDOWN does not trigger a powercycle. Using a signal generator and triggering PWRDOWN with a 20ms pulse, does indeed trigger a powercycle of PMIC.

    So I believe the 2 following questions still remain:

    What is the minimum pulse time needed for PWRDOWN pin, in order to do a power cycle of PMIC?

       How much can this minimum pulse time vary between different devices and in worst case?

  • Florin,

    It looks like I misspoke on this topic originally. In further discussion with the team, there is a 15ms debounce time on the PWRDOWN pin. We do not have a maximum spec for this item. For a faster shutdown reaction, I recommend using RESET_IN or POWERHOLD to turn off the device.

    Thanks,

    Nastasha

  • Hello,

       Thanks for the clarification. I'm focusing now to extend the pulse width with a monostable circuit.

     

    About the debounce on PWRDOWN pin being 15ms,  I couldn’t find this information in the datasheet or application notes.  Where is this documented please?

    Is this debounce fixed or SW programmable ?   If SW programmable, what registers?

     

    I need this information to properly dimension the pulse extend circuit.

     

    Thanks a lot!

     

    P.S.:       1. PMIC device code we’re using is TPS6590378ZWS.

                    2. There is no debounce time mentioned in the PMIC datasheet Table 5-11. Is that correct?

     

     Regards,

      Florin

  • Florin,

    Hi, this is a fixed debounce, not programmable. I noticed as well that it is not clearly documented anywhere. I have flagged this as something to include in the next datasheet revision.

    Thanks,

    Nastasha