This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25155: can i have BQ25155 minus LDOs

Part Number: BQ25155

We are using the BQ25155 charger. We love ship mode, battery protection, and battery level measurement or battery voltage tracking offered by the chip. However, we are not using the 150mA LDO and 10mA LDO. Can we have BQ25155 without the LDOs? Does any other charger chip do this? If we can reduce pin counts, it's better for the design complexity. 

Note: we also love the low power characteristic of BQ25155, and that's why we selected it. So any charger proposed should have equal power consumption or better in power consumption than the BQ25155.