Hello,
In the datasheet the recommended output capacitance for the TLV62585 dc/dc converter with a 1uH inductor is 47uF.
I want to use this part with a 5V input and 3.8V output, to power a GSM module. The GSM module has a capacitance on it's input of ( 470uF x 2 ). This capacitance will essentially sit on the output of the TLV62585 part.....will this pose as a problem ? If this part is not suitable, please advise.
Regards,
Eben