Part Number: BQ27220
Other Parts Discussed in Thread: BQSTUDIO,
Hi Team,
Here need your help to have the suggestion or comment for the bqstuido application questions:
1. Can't charging voltage and temperature and there will have a red warning words (A read of data written failed comparison).
2. Can’t find the GPC packager from bqstudio
Follows items we did ask and been checked by customer.
*Is it only this item can’t change? But others are okay like as temp low / temp high.
--> Can’t change the temperature in Safety Column also
*What’s real Battery voltage now?
-->Did check two battery parts :38V/3.3V
*Suggest you turn off Auto refresh function during the setting.
--> Turn off Auto refresh and the result is the same
*Check and make sure the setting is unseal
-->From above item (SEC1, SEC0 : 10), It’s unseal.
3. Please refer attached file for the detail including the *.gg file.
BQ27220 bqStudio application question 05292020 A AL.pptx
Best regards,
Albert Lee.
.