Hi there,
In various application notes I come across 2 formulae to calculate the primary inductance of a flyback transformer.. These 2 formula are given below :-
a) Lp = (Vin min² x Dmax² x effeciency) / (2 x Freq x Po). where Vin min = min input DC voltage, Dmax = max duty cycle, Po = output power, Freq = freq of operation.
b) Lp = Lsec (Np/Ns)², where
Lsec = (Vo+Vf)(1-Dmax) / (ΔIsec x Freq). where Vo = output voltage, Vf = voltage drop of output diode,
where ΔIsec = (Io x 0.3) / (1-Dmax), where Io is output current
Np/Ns = (Dmax) / (1-Dmax) x (Vin min) / (Vo = Vf)
My question is that if i apply formula given in first equation , i get a particular value of Lp and when I derive the Lp using the second set of equations i get a VASTLY different value for Lp (much higher that Lp derived from 1st equation)
This has left me confused
Kindly advise correct equation to derive Lp for a flyback transformer
Regards
Atul Bhakay