This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27520-G4: Is Learning Cycle needed after getting the report from GPC?

Part Number: BQ27520-G4

It is successful to get the report from GPC.
My Best chemical ID was 2019
I will generate Golden file with chemical ID 2019.
Then do I need to do Learning Cycle (document ID:SLUA902, 2.6) even when using this Golden file?
If it is yes, is this cycle needed for all boards individually for example Mass products?

Best Regards,

Yuichi Tsutsui