Other Parts Discussed in Thread: TPS74801
I am trying to figure out which 1.5A regulator to use. Specifically where x= 2, 3, 8.
I am looking for a ULDO linear regulator for 1.2Vin and 1.0Vout at about 1A. The 1.0V rail is an analog rail to a 10Gbps device with IMPOSSIBLE to meet noise requirements (floor of 2.5nV/rtHz from 0 to 300MHz). I want to get as low noise as possible. The 1.2V is from a POL buck switching at 600kHz.
It looks to me that the 74301 has better PSRR but higher noise at 74801. Not really sure how the 74201 fits in to the equation.
Solution cost and size are relatively unimportant to me (I will be using lots of Cout).
Why do all 3 parts exist and why would I pick one over the other?
Fortunately, if I stick with the 5x5 QFN, they look to be pin compatible.