This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53319: About FCCM mode setting

Part Number: TPS53319


Hi TI Team,

I want to confirm the connection setting for TPS53319 FCCM mode.

In the datasheet it says it should be connected to PGOOD pin, but didnt mention to pull it up with VREG.

The circuit for EVB shows it is pull up with 100kohm to VREG.

So is the connection in EVB correct?

Thanks