Other Parts Discussed in Thread: TPS63710
Dear Sir/Madam,
I have a board that is fully TI and the +4V5 DC/DC (TPS62150) keeps getting damaged during power-on.
Three out of three boards have failed. Some powered a few times before failing.
The devices are:
(1) TPS25940AQRVCRQ1 for input protection. +12V input.
(2) TPS62150 for +12V to +5V5
(2.1) TPS7A4701 for +4V5. Load current = 0.5A
(3) TPS63710 for +12V to -5V5
(3.1) TPS7A3301 for -4V5. Load current = 0.5A
I have pulled of the TPS62150 and connected a bench supply to input of TPS7A4701 and the board power and functions fine.
I have looked at the TPS63710 to TPS7A3301 power-on and it looks fine. The start-up time is about 50ms.
I cannot check the TPS62150 power-on however the SS/TR capacitor is 3n3F approx. 1.65ms.
Only the TPS62150 gets damaged. What could possibly cause the TPS62150 to get damaged?
Regards Joe