This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62568A: How to calculate VFB @ 125C, and any issue to change inductor value.

Part Number: TLV62568A

Hi,

My customer is thinking how to calculate MAX VFB at Tj=125C as follows. Is this method correct? Please let us know.
 TLV62568A datasheet said VFB at Vin=5V/Tj=25C is Min:0.588V / Typ:0.6V / Max:0.612V. Also, we can find the graph of "VFB vs Tj".   According this graph, Diff of VFB between Tj=25C and Tj=125C is 0.00015V.   So MAX VFB @ Tj=125C is 0.612+0.00015=0.61215.

My customer wants to change inductor value from recommended 1uH to 1.5uH or 2.2uH. What problem does this cause?  Please advise us.

Thanks and best regards,
M.HATTORI.