Hi,
we need to drive a green LED capable of 20A at ~3.5V. We are implementing the design in the board linked below.
http://www.ti.com/tool/PMP8016
It seems to be perfect for our needs.
Pulse requirements is:
2ms ON at max current (20A)
8ms OFF
Duty-cycle is 20%.
Questions:
(1) is it possible to run the board at 24Vdc, or there is a limit? For sure we will considering to use higher Vds mos.
(2) is the circuit able to run at that duty cycle? I'm not sure it can run in continuous way since in the various examples we see only "high frequency PWM mode" with Ton of some tens of [us]... in my design i need 2ms.
(3) the MOS that shunts the LED must be dissipated since it sinks 20A for the 80% of the time, right? During that time, it dissipates: Rds,on * I * I = (few mohms) * 20 * 20 [W] >>> few Watts ... Is it right?
(4) why there is only 1 MOS for the upper side and 2 for the lower side? Maybe because the top side requires small current, while the bottom side requires synchronous rectification of many Amps???
Thanks in advance