Other Parts Discussed in Thread: TPS54202, LM5088, TPS560430
Hi,
we observe the same problem as described in the related thread.
The pcb contains 5 buck converters:
1) TPS54302: 24V => 3,3V
2) TPS54202: 24V => 5V
3) TPS54202: 24V => 15V
4) LM5088: 24V => -15V
5) TPS560430: 24V => 12V
Assembly variant A contains 1) only.
Assembly variant B contains 1)-4) only.
Assembly variant C contains 1)-5) only.
In variant A TPS54302 brokes very often if hot plugged to a laboratory power supply with 24V.
I have observed this while initial testing of 5 boards with no load at the output.
With other assembly variants it doesn't occur. I assume due to the other input capacitors in parallel.
After finding Shawns answer in the related thread hot plugging to 24V was avoided and the problem is gone.
It was plugged to 10V and than the voltage was raised to 24V.
In the real product it is powered with a 500W Meanwell power supply, which maybe can also have a high dU/dt while power up.
So I'm afraid, that i will breake again in the real product. Are there recommendations how to avoid this reliable?
Is it to be expected, that only a large spike on the input could be the root of the problem?
I don't expect a spike for the laboratory power supply with current limiter set to some 100mA.
Before testing that, which will most likely break it again i would like to know if there are other know issues.
Or in other words. Would you expect this problem if hot plugged to a 24V truck battery?
Thanks,
Jochen