Other Parts Discussed in Thread: BQSTUDIO
Hello,
I'm currently using the BQ35100 with non-rechargeable cells on a board. I'm using the accumulator mode.
Conf A : 0x80 (same as default value)
After the calibration i'm doing a "New_Battery()" to reset the "AccumulatedCapacity".
My issue is that, on some boards the "AccumulatedCapacity" counter is increase from 0 to 4,29E9 and some times on others/sames boards it's decrease (start at 0 and roll over to 4,29E9) 4,29E9 to 0. (Same hardware, not able to charge the cells).
Regards,
Goulwen LE BOZEC.