Part Number: LM5181
Other Parts Discussed in Thread: LM5180
Hi there,
I want to design dual output dc to dc isolated converter
my input range is 12 - 65 volt and output1 DC : 5v@750 mA output2 DC : 5V@10 mA
I got design form web-bench for one output and i learnt from 5181 eval board by simply adding one more winding dual output design is possible.
so while studying I seen table which says output current varies with input voltage. i have attached that table here
my question
1. what this table about?
2. Does output current is not constant and really depend on input voltage?
3. I need continuous load current of 750 ma and 10 ma irrespective of input voltage is this possible with 5181 or any other device will support