Other Parts Discussed in Thread: LM5176
I have an LM5176-Q1 design which creates 40V from a 24V input. With no load, the voltage properly comes up to 40V. This design also uses a shunt regulator to prevent back emf from a DC motor. The shun regulator has 4 2200 uF aluminum electrolytic capacitors. When the shunt regulator is attached, the voltage only get to 15V. I tried slowing down the ramp by changing Css to 0.33 uF to give a soft start time of 50ms. This seemed to help on one board but it is inconsistent. When I show the capacitance on the output in webench, it says that the phase margin is too low. Changing the compensation capacitor helps with the error but not the functionality. What can be done to slow the ramp so that the charging of these large capacitors does not prevent the supply from coming up?2818.MotorVoltage.pdf