Hi Andy-san,
The following are reports and inquiries from customers.
Ra Table was returned to the initial value in the two units that were refreshed (completely discharged → fully charged).
When refreshed, the remaining amount gauge IC itself will be in a non-energized state and will be reset when it is completely discharged.
Is it possible that Ra Table became the initial value following this reset?
(I think that the operation method to occasionally remove the battery pack is within the assumption, so it is unlikely that the data will easily return to the initial value.)
Or, since the battery is not so deteriorated, the battery was activated during the process of full discharge → full charge, and the result better than the initial value of the original Ra Table (low impedance result) was obtained, but as a result, Is it possible to think that the initial values of Ra Table have been adopted?
(For example, when the initial value is 40 mΩ and the battery was 60 mΩ during the charging/discharging process, when it is measured as 20 mΩ after complete discharge → full charge, 20 mΩ is discarded and it is imagined to learn as 40 mΩ.)
Best regards,
Kagawa