HI All
Could you review LM5176 SCH?Thanks a lot
Board environment: car equipment.
The power supply voltage range is 9-36V, the output voltage is 12V, and the maximum current is 6A. Ambient temperature -40℃-85℃, only use PCB for heat dissipation.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI All
Could you review LM5176 SCH?Thanks a lot
Board environment: car equipment.
The power supply voltage range is 9-36V, the output voltage is 12V, and the maximum current is 6A. Ambient temperature -40℃-85℃, only use PCB for heat dissipation.
Hi Seasat,
Thanks for reaching out with your question and for considering the LM5176 in your design.
As a first step of the review, it is recommended to use the LM5176 quick-start calculator to double check the component values. This will help catch most mistakes. After that is complete I will do an in depth review of the schematic.
Thanks,
Garrett