This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65950 TPS65930 TPS65920: VREF connection



Q: Does VREF need a capacitor?

A: Yes, this pin should be connected to a 1uF cap to GND. This is the main reference voltage for all internal blocks. During power up if the device doesnt power this should be the first pin to check. This should be at 0.75V

If this is not 0.75V then something is missing and the board is not getting correct power.