This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5007: failed -5V generation via IBB

Part Number: LM5007


I converted the LM5007 into an inverting buck-boost to get a negative output voltage of -5V from a +24V input supply voltage.

Following TI's application report about how to work with IBBs, I created this circuit to obtain the +24V to -5V - conversion:

The problem is, that at the output there aren't the desired -5V, it only reaches about -4V.

In operation with a load I got these signals as a result:

Vout (output voltage) SW (switching node) BST (bootstrap)

Well, I don't understand why the On- and Off-Time is not going to be adjusted correctly, so that the IBB regulates a -5V output. (attached also an on-time measurement)

Maybe someone has an advice to solve this problem or an idea where there might be an error.