This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61196: Driving two LED strings with different Voltages

Part Number: TPS61196


Hello there,

We plan to use part TPS61196 to drive below LEDs:

  • RED string of 28 LEDs with Vf =2V for a total of 56V
  • BLUE string of 28 LEDs with Vf =3.1V for a total of 86.8V

Is this possible with this part ? 

If not, can you help suggest a suitable solution ?

Appreciate your response.

Thank you.

Regards,

Ryan